LPC 1769 express board FreeRTOS BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1769 express board FreeRTOS BSP

1,157件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Thu Aug 21 18:55:22 MST 2014
Product 1. LPC1769 expresso board and LPCexpresso base board,  IDE: LPCEXpresso , RTOS: FreeRtos

1. I try with  "LPC1769_FreeRTOS_Plus_Featured_Demo_002" and it is working fine
2. i try with "lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769" with FreeRtos demo and is working fine
3. I implement few example in boath enviorment and are working well

I try to bring one example to from 2 system to 1 st system then find out it is not compatible eachother, they way write LPC low level Library are different

example 1 ; use
1. CMSISv2p00_LPC17xx
2. lpc17xx.cmsis.driver.library

example 2; use
1. lpc_chip_175x_6x
2. lpc_board_nxp_lpcxpresso_1769

My qustion to LPCOPen software team members:
Q: What is your future direction ?

My proposal is to develop application directory

1. Cortex M0/M3/M4  folder
2. LPC xxxx  chip folder
3. Board
4. RTOS folder
5. middle ware
6. Application

Then easy for the developers to pick and choose their system and easy to move between Chip to Chip, board to board, RTOS to RTOS etc



ラベル(1)
0 件の賞賛
返信
0 返答(返信)