LPC 1768 & LAN 9354 PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1768 & LAN 9354 PHY

1,869件の閲覧回数
jayasankarrv
Contributor I

On a new project we are going to use LAN 9354 Ethernet switch (http://ww1.microchip.com/downloads/en/DeviceDoc/00001926B.pdf ) along with LwIP. We are using LPC 1768 MCU, is there any reference code for the PHY for this chip or any available sources which is similar to LAN 9354 which can be used in conjunction with LwIP & LPC 1768#

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,624件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Jayasankar R V,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

To provide the fastest possible support, you can refer to the Ethernet demos in the CMSIS library for details.

lpc175x_6x_cmsis_driver_library_0.zip - Google Drive 

TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 件の賞賛
返信