LPC1778 P0[24],P0[25]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778 P0[24],P0[25]

1,220 Views
yukinobuhori
Contributor II

Is it possible to PULL-UP P0 [24], P0 [25] of LPC1778?
There was no change in PINSEL_SetPinMode (0, 24, 2).

0 Kudos
Reply
1 Reply

1,154 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Yukinobu Hori ,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
I was wondering if you can disclose more details about the issue, for example, complete code, screenshot of register, etc.
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 Kudos
Reply