LPC 1768 & LAN 9354 PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 1768 & LAN 9354 PHY

1,864 Views
jayasankarrv
Contributor I

On a new project we are going to use LAN 9354 Ethernet switch (http://ww1.microchip.com/downloads/en/DeviceDoc/00001926B.pdf ) along with LwIP. We are using LPC 1768 MCU, is there any reference code for the PHY for this chip or any available sources which is similar to LAN 9354 which can be used in conjunction with LwIP & LPC 1768#

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,619 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Jayasankar R V,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

To provide the fastest possible support, you can refer to the Ethernet demos in the CMSIS library for details.

lpc175x_6x_cmsis_driver_library_0.zip - Google Drive 

TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 Kudos
Reply