LPC 1519 watchdog reset not happening correctly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1519 watchdog reset not happening correctly

1,391件の閲覧回数
ravalimuppalla
Contributor I

Hello,

I am trying to wake the Micro, 1519, from power down after WFI with a watchdog. I change the time in TC then put it to power down. So after TC amount of time i expect a reset from watchdog. But when i check the reset status it gives me a POR and not a watchdog reset. 

LPC_WWDT->TC = 2 minutes;  //previously the time was for 33sec

LPC_WWDT->MOD = 0x23; 

disable_irq;

WFI;

enable_irq;

After reset i check the reset status with Chip_SYSCTL_GetSystemRSTStatus(); and i get a POR.

I tried "Chip_SYSCTL_EnableERP0PeriphWakeup(SYSCTL_ERP0_WAKEUP_WDTINT)" which wakes the micro but i don't get a reset on wake up, instead the micro waits for 90 seconds before getting reset. Then the reset status is watchdog reset.

Is there any reason for this?

Thanks!

タグ(3)
0 件の賞賛
返信
1 返信

1,288件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ravali Muppalla ,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

To provide the fastest possible support, I'd like to recommend you to refer to the periph_wwdt demo in the LPCOpen library.

LPCOpen Software for LPC15XX|NXP 

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信