LCPXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCPXpresso

4,814 Views
yukinobuhori
Contributor II

When debugging with LPCXpresso IDE and LPC-Link
The following error occurs.

LPCXpresso: Error =>
cannot run program "wmic": createProcess error = 2, The system cannot find the file specified.

There were no errors in August. Then various installations
I am updating. Are they the cause?

How can I get rid of the error?

0 Kudos
Reply
5 Replies

4,742 Views
yukinobuhori
Contributor II

Thank you.
With reinstall and review of PATH
I'm back.

0 Kudos
Reply

4,786 Views
converse
Senior Contributor V

You should be using MCUXpresso (not LPCXpresso, which is more than 5 years old now).

Download from

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-i...

0 Kudos
Reply

4,805 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello yukinobuhori,

How about delete the .metadata folder under workspace, then open IDE, open a simple project, try to debug. 

 

BR

Alice

0 Kudos
Reply

4,800 Views
yukinobuhori
Contributor II

Thank you.
I worked as instructed, but it was the same.

0 Kudos
Reply

4,769 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

How about reinstall it ? Or I also recommend MCUXpresso if you can.

 

BR

Alice

0 Kudos
Reply