LCDVDx pins Datamapping change possible?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCDVDx pins Datamapping change possible?

2,109件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GokhanZorbeyOzcan on Tue Nov 15 08:35:37 MST 2011
Hello All,
I will be using LPC3250 for a cu::stom board. That board will be able to drive several TFT-LCD panels. Both  16 bit 1:5:5:5 mode and  24 bit 8:8:8 mode will be used. For the purpose of having an easy hardware design, are there any ways to change the Data Mapping of LCD module to LCDVDx pins?
Best Regards
Gokhan Ozcan
ラベル(1)
0 件の賞賛
返信
1 返信

2,025件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Magicoe.Niu on Thu Dec 06 19:58:31 MST 2012
Hi,

Seems LPC3250 LCDVx pins is quite easy to compatible 16bit and 24bit lcd data bus, using the highest 5bit is enough. Attached is pin map, fyi.

B.R.

Magicoe
0 件の賞賛
返信