LCD interfacing with ARM cortex M0+ lpc845

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LCD interfacing with ARM cortex M0+ lpc845

6,491 次查看
vidhya1
Contributor III

Hi,

I'm trying to interface 8x2 lcd using parallel interfacing[4 bit mode], Display used - 8x2 lcd [PC 0802--A] ST7066U--Dot Matrix LCD Controller/Driver

Since i'm trying to interface using GPIO pins, not using I2C or SPI interface, and since no drivers are there for this particular MCU[LPC845], I compared with lpc2148 MCU [lcd.c and lcd.h files], and have made the changes, but not able to write to the display.

And when checked the data/command signals in the oscilloscope, in data pins I'm getting float voltages[i.e., for d4-D7] LOW signal on this pins, and high signals on command pins[RS,RW,EN].

Kindly suggest me the process of writing the char/string to the display varies for ARM mcu?as i'm referring lpc2148 libraries.

Thank you

标签 (1)
7 回复数

6,052 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The LPC845 does not have LCD interface, you would like to use GPIO to simulate the LCD timing so that you can write data to the LCD display.

Can you use the LPC family which has LCD interface for example LPC54xxx for example LPC54608?

LPC546XX Microcontroller (MCU) Family | NXP 

If you do want to use the LPC845, can you post the LCD data sheet so that we can check the LCD interface timing?

BR

Xiangjun rong

6,052 次查看
vidhya1
Contributor III

Yes sir I'm using GPIO's for interfacing and writing data to display, since we have started

working on LPC845 mcu, is there any other MCU compatible to this and there 8x2 LCD

display used?

I have attached the datasheet and the code for reference.

Please suggest me on this.

https://wetransfer.com/downloads/89da07604cfdcbf426978a1300994de220190314105349/09a6b71f312b14490048...

Thank you

0 项奖励
回复

6,052 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You have to configure the GPIO pins as GPIO output mode, you can set and clear the pins as you expected.

Firstly, you have to enable the GPIO clock.

Pls refer to the section 8.6.22 System clock control 0 register. For example, you can set the GPIO0 clock with the code:

SYSCON->SYSAHBCLKCTRL0|=1<<6|1<<20|1<<18; //enable the GPIO0, GPIO1 and IOCON modules clock

SYSCON->PRESETCTRL0|=1<<61<<20; //clear GPIO reset, the line may be unnecessary

Then you can set the GPIO direction register

GPIO->DIR[0]|=1<<(GPIOPinIndex);

then you can set/clear the pin

//set pin

GPIO->SET[0]=1<<(GPIOPinIndex);

//clear pin

GPIO->CLR[0]=1<<(GPIOPinIndex);

Pls have a try

Hope it can help you

BR

Xiangjun Rong

5,220 次查看
tdaniel
Contributor I
Hello friends I'm looking for a tutorial for connect with lpc845 and LCD16X2, can you help me, please? 
0 项奖励
回复

6,052 次查看
vidhya1
Contributor III

Sir thanks for the explanation, before trying this I had changed for below configuration registers

    LPC_SYSCON->SYSAHBCLKCTRL0 |= (WKT|MRT|GPIO);
    LPC_SYSCON->SYSAHBCLKCTRL[0] |= GPIO1;
    LPC_SYSCON->SYSAHBCLKCTRL[0] |= GPIO0;

And after I compiled with the above changes getting junk/characters on display, then again

added the above configuration to try with the configuration for the GPIO clock you suggested,

but getting blank display, so cross checking with the data pins again.

Thank you

0 项奖励
回复

6,052 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you connect the GPIO pin to a oscilloscope and check if the GPIO toggles after you set/clear the GPIO pins by code, if the GPIO pin toggles, it means that the code is okay.

BR

XiangJun Rong

0 项奖励
回复

6,052 次查看
vidhya1
Contributor III

Ok sir will check it, but kindly tell me

all 4 data pins[d4-d7] used should toggle?

And what should be the status of RS,RW,EN port pins?

It should remain high[control pins]? Please confirm

Thank you

0 项奖励
回复