LCD Driver PCF2119 Sample Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD Driver PCF2119 Sample Code

2,372件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alan_nn on Tue Apr 01 21:46:12 CDT 2014
The PCF2119x is a low power CMOS LCD controller and driver, designed to drive a dot matrix LCD display of 2-lines by 16 characters or 1-line by 32 characters with 5x8 dot format. These sample code demonstrate how to configure the display method and operating mode of PCF2119 , and how to show the character on built-in character set, also how to generate User-Defined charaters and show on the screen.Example for the message: "NXP" "2014 WELCOME" "yours coming" .Customized big chinese character:"新年" "快乐".
ラベル(1)
0 件の賞賛
返信
1 返信

2,199件の閲覧回数
longoal025
Contributor I

Where is the Code?

0 件の賞賛
返信