LAN8720A Issues (SOLVED)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LAN8720A Issues (SOLVED)

12,519 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jnewell on Mon Sep 09 08:15:57 MST 2013
Hello, I'm just wondering if anyone out there has created a custom board with a LAN8720A.
I'm having problems with getting the 25MHz crystal to run.
I have attached the schematic that I am using.

Any Help/info would be appreciated.

Thanks,
Josh
标签 (1)
0 项奖励
回复
24 回复数

422 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Tue Sep 10 16:42:20 MST 2013
For what it's worth, this is the ethernet part of our custom PCB. It is working.
Please don't ask me about it as I am not a hardware guy -- I do the firmware.

BTW, read the LAN8720 about mode etc. settings and compare with the pullups
and pulldowns on the schematic.

PS. We are connecting to an LPC1778 (208 QFP) so some of the CPU labels may
need translating for whatever chip that you are using.

PS. I think the forum reduced the jpg by about 19% -- Oh well!

Hope this helps, Mike
0 项奖励
回复

422 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jnewell on Mon Sep 09 08:37:42 MST 2013
Also, I have noticed that at the VDDCR pin I am reading a voltage of 2.0V. According to the datasheet the internal regulator should be outputting 1.2V. Not sure why I'm getting 2.0V, any ideas?

-Josh
0 项奖励
回复

422 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jnewell on Mon Sep 09 08:26:13 MST 2013
Yes I sure have,

I have an RDB1768 eval board (LPC1768 + LAN8720A) that I based my design on, and the schematic is pretty much the same besides the bead separating the analog 3.3V from the main 3.3V power rail (the PHY_A3V3 that is supplied to VDD1A and VDD2A). This shouldn't be an issue, though.

Thanks,
0 项奖励
回复

422 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Mon Sep 09 08:22:24 MST 2013
Hello Josh,

have you already googled for "LAN8720A NXP". Here is e.g. one hit:

http://www.element14.com/community/servlet/JiveServlet/download/38-106658

I think also some LPCXpresso have the LAN8720A on board?

Best regards,

Martin
0 项奖励
回复