Keil LPC1114 Evaluation Board with LPC1112FHN24 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Keil LPC1114 Evaluation Board with LPC1112FHN24 processor

1,374件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rihana N. on Wed Nov 05 02:06:02 MST 2014
Hi,

According to the nxp site : http://www.nxp.com/demoboard/OM11086.html#products , LPC1114 evaluation board is available for processor LPC1112FHN24. I have searched many online sites, but all of them have the evaluation board populated with the  LPC1114FBD48/302 device. Can anyone tell me how I can place an order for this evaluation board which is populated with LPC1112FHN24 processor?

Thanks,
Rihana
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,368件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rihana N. on Wed Nov 05 20:07:02 MST 2014
Hi starblue,

Thank you for that clarification.
0 件の賞賛
返信

1,368件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Wed Nov 05 02:54:18 MST 2014
I think you are misunderstanding that LPC1112FHN24 is in the list of related products.

The idea is to start development with LPC1114FBD48/302 and then later move on to your specific processor when your own board is ready. The processors are so similar that no real porting is needed. You just need to make sure you don't use resources that are unavailable on the LPC1112FHN24.

(Hey LabRat, you could be a little more friendly to newbies.)
0 件の賞賛
返信

1,368件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Nov 05 02:25:14 MST 2014
:quest:

You are not really asking if Keil is selling a board with LQFP48 MCU package and a HVQFN24 MCU on it?
0 件の賞賛
返信