KEIL Software pack installer LPC2103

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEIL Software pack installer LPC2103

Jump to solution
7,703 Views
oykr
Contributor II

Hi. Have an old board that I need to write code for an LPC2103. Accoridn to ARM KEIL uVISION supports the LPC2103 https://www.keil.com/dd/chip/3974.htm but I cannot find it in the PACK INSTALLER device list. Do I manully need to add the LPC2103 software packs?

Tags (3)
0 Kudos
Reply
1 Solution
7,673 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @oykr 

Device family packs have only been created for Cortex-M based devices. For these older devices  the "legacy support" files need to be installed:

https://developer.arm.com/documentation/101407/0541/Creating-Applications/Tips-and-Tricks/Use-MDK-Ve...

Kind regards,

Alice

View solution in original post

4 Replies
7,683 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @oykr 

I have already submitted the issue to ARM. I will send you with any updates. You can also ask arm if have any other issue with KEIL. 

https://www.keil.com/  

 

BR

Alice

0 Kudos
Reply
7,673 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @oykr 

Device family packs have only been created for Cortex-M based devices. For these older devices  the "legacy support" files need to be installed:

https://developer.arm.com/documentation/101407/0541/Creating-Applications/Tips-and-Tricks/Use-MDK-Ve...

Kind regards,

Alice

6,895 Views
oykr
Contributor II

Hi

I  downloaded and installed the leacy pack for 

But I can still not see it in my DEVICE list in the keil uvisin PACK INSTALLER. How do I import the device into the PCCK INSTALLER. DO I need to goto FILE -> IMPORT FROM FOLDER...  ?

What File or  file estension am I looking for in that folder?

I am not an experienced firmware developer, only an expert PCBA desinger who need to write some simple code to test&verify my hardware

 

KR

Øystein

0 Kudos
Reply
6,893 Views
oykr
Contributor II

Hi

OK, think I found why. I only have the MDK-LITE license

And on https://www2.keil.com/limits it states:

 

  • Arm7/Arm9/Cortex-R4 devices are not supported.

I guess thats why, unless there is a workaround

KR

Oystein

0 Kudos
Reply