KE04 RTC accuracy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KE04 RTC accuracy

跳至解决方案
2,272 次查看
jun1
Contributor V

HI.

Thank you for your help.
How accurate is the RTC when a bus clock is used as the RTC clock source?

I looked at the KE04 Sub-Family Data Sheet, but is it ±5% (T = 25 °C, VDD = 5 V) for 37.5 kHz?

jun.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,236 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jun,

The RTC module is a frequency divider, it's accuracy is totally dependent on the the clock source accuracy. So if you use BUS clock as RTC driving clock source, pls check if you use 37.5 internal IRC or external crystal.

If you use 37.5KHz IRC as RTC clock source, the 37.5KHz IRC after  Factory trimmed is +/-0.5%, I think it is  the RTC accuracy.

Hope it can help you

BR

XiangJun Rong

在原帖中查看解决方案

2 回复数
2,237 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jun,

The RTC module is a frequency divider, it's accuracy is totally dependent on the the clock source accuracy. So if you use BUS clock as RTC driving clock source, pls check if you use 37.5 internal IRC or external crystal.

If you use 37.5KHz IRC as RTC clock source, the 37.5KHz IRC after  Factory trimmed is +/-0.5%, I think it is  the RTC accuracy.

Hope it can help you

BR

XiangJun Rong

2,236 次查看
jun1
Contributor V

Thank you for your reply.

37.5 uses internal IRC so factory trimmed value is +/- 0.5%.

OK.

Thank you very much.
have a good day.


Jun.

0 项奖励
回复