KE04 RTC accuracy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE04 RTC accuracy

Jump to solution
2,409 Views
jun1
Contributor V

HI.

Thank you for your help.
How accurate is the RTC when a bus clock is used as the RTC clock source?

I looked at the KE04 Sub-Family Data Sheet, but is it ±5% (T = 25 °C, VDD = 5 V) for 37.5 kHz?

jun.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,373 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jun,

The RTC module is a frequency divider, it's accuracy is totally dependent on the the clock source accuracy. So if you use BUS clock as RTC driving clock source, pls check if you use 37.5 internal IRC or external crystal.

If you use 37.5KHz IRC as RTC clock source, the 37.5KHz IRC after  Factory trimmed is +/-0.5%, I think it is  the RTC accuracy.

Hope it can help you

BR

XiangJun Rong

View solution in original post

2 Replies
2,373 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jun,

The RTC module is a frequency divider, it's accuracy is totally dependent on the the clock source accuracy. So if you use BUS clock as RTC driving clock source, pls check if you use 37.5 internal IRC or external crystal.

If you use 37.5KHz IRC as RTC clock source, the 37.5KHz IRC after  Factory trimmed is +/-0.5%, I think it is  the RTC accuracy.

Hope it can help you

BR

XiangJun Rong

2,373 Views
jun1
Contributor V

Thank you for your reply.

37.5 uses internal IRC so factory trimmed value is +/- 0.5%.

OK.

Thank you very much.
have a good day.


Jun.

0 Kudos
Reply