JavaScript Error in Time Series Studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JavaScript Error in Time Series Studio

跳至解决方案
2,526 次查看
Bay
Contributor III

Hi, I am using the LPC55S69 EVK board and test on time series studio (latest version), but sometimes (data logging, emulation) it will prompt this error.

Please assist.

Bay_0-1748337378651.pngBay_0-1748337378651.png

 

0 项奖励
回复
1 解答
2,489 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

Did you turn off eIQ Portal when using Time Series Studio?

Please do not turn off eIQ Portal when using Time Series Studio.

BR

Harry

在原帖中查看解决方案

4 回复数
2,500 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

 (data logging, emulation) it will prompt this error.

May I ask if this error frequently occurs?

We want to reproduce this issue.

But according to the error message.

Uncaught Exception:
Error: EPIPE: broken pipe, write

This typically indicates that the main Node.js process tried to write to a stream (like a file, socket, or pipe) that was already closed or unexpectedly disconnected.

BR

Harry

 

0 项奖励
回复
2,496 次查看
Bay
Contributor III

Hi Harry, 

Yes, it occurs frequently. Now I am training the data, and it keeps prompting this error.

Bay_1-1748415360162.pngBay_1-1748415360162.png

And also, when programming the time series studio firmware, it also keeps prompting this error. But at the end, it programs successfully.

Bay_2-1748415446310.pngBay_2-1748415446310.png

 

 

 

0 项奖励
回复
2,490 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

Did you turn off eIQ Portal when using Time Series Studio?

Please do not turn off eIQ Portal when using Time Series Studio.

BR

Harry

2,487 次查看
Bay
Contributor III

Hi Harry,

I closed the eIQ Portal when using Time Series Studio.

I've reopened it, and the error hasn't been prompted so far.

Thanks for the quick response!

0 项奖励
回复