JavaScript Error in Time Series Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JavaScript Error in Time Series Studio

ソリューションへジャンプ
2,764件の閲覧回数
Bay
Contributor III

Hi, I am using the LPC55S69 EVK board and test on time series studio (latest version), but sometimes (data logging, emulation) it will prompt this error.

Please assist.

Bay_0-1748337378651.png

 

0 件の賞賛
返信
1 解決策
2,727件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

Did you turn off eIQ Portal when using Time Series Studio?

Please do not turn off eIQ Portal when using Time Series Studio.

BR

Harry

元の投稿で解決策を見る

4 返答(返信)
2,738件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

“ (data logging, emulation) it will prompt this error.”

May I ask if this error frequently occurs?

We want to reproduce this issue.

But according to the error message.

Uncaught Exception:
Error: EPIPE: broken pipe, write

This typically indicates that the main Node.js process tried to write to a stream (like a file, socket, or pipe) that was already closed or unexpectedly disconnected.

BR

Harry

 

0 件の賞賛
返信
2,734件の閲覧回数
Bay
Contributor III

Hi Harry, 

Yes, it occurs frequently. Now I am training the data, and it keeps prompting this error.

Bay_1-1748415360162.png

And also, when programming the time series studio firmware, it also keeps prompting this error. But at the end, it programs successfully.

Bay_2-1748415446310.png

 

 

 

0 件の賞賛
返信
2,727件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

Did you turn off eIQ Portal when using Time Series Studio?

Please do not turn off eIQ Portal when using Time Series Studio.

BR

Harry

2,725件の閲覧回数
Bay
Contributor III

Hi Harry,

I closed the eIQ Portal when using Time Series Studio.

I've reopened it, and the error hasn't been prompted so far.

Thanks for the quick response!

0 件の賞賛
返信