JavaScript Error in Time Series Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JavaScript Error in Time Series Studio

Jump to solution
2,503 Views
Bay
Contributor III

Hi, I am using the LPC55S69 EVK board and test on time series studio (latest version), but sometimes (data logging, emulation) it will prompt this error.

Please assist.

Bay_0-1748337378651.pngBay_0-1748337378651.png

 

0 Kudos
Reply
1 Solution
2,466 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

Did you turn off eIQ Portal when using Time Series Studio?

Please do not turn off eIQ Portal when using Time Series Studio.

BR

Harry

View solution in original post

4 Replies
2,477 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

 (data logging, emulation) it will prompt this error.

May I ask if this error frequently occurs?

We want to reproduce this issue.

But according to the error message.

Uncaught Exception:
Error: EPIPE: broken pipe, write

This typically indicates that the main Node.js process tried to write to a stream (like a file, socket, or pipe) that was already closed or unexpectedly disconnected.

BR

Harry

 

0 Kudos
Reply
2,473 Views
Bay
Contributor III

Hi Harry, 

Yes, it occurs frequently. Now I am training the data, and it keeps prompting this error.

Bay_1-1748415360162.pngBay_1-1748415360162.png

And also, when programming the time series studio firmware, it also keeps prompting this error. But at the end, it programs successfully.

Bay_2-1748415446310.pngBay_2-1748415446310.png

 

 

 

0 Kudos
Reply
2,467 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Bay 

Did you turn off eIQ Portal when using Time Series Studio?

Please do not turn off eIQ Portal when using Time Series Studio.

BR

Harry

2,464 Views
Bay
Contributor III

Hi Harry,

I closed the eIQ Portal when using Time Series Studio.

I've reopened it, and the error hasn't been prompted so far.

Thanks for the quick response!

0 Kudos
Reply