JTAG flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG flash

3,714件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gritho on Fri Feb 07 02:06:40 MST 2014
Hi!

I need to flash/program and debug custom PCB with ARM Cortex M0 (LPC11C24) on board.

I have required JTAG pins, but I don't know how connect them to my
computer and flash/debug my programs.

Do you have some advices and which of your products could I use?

Thanks a lot!
ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,666件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gritho on Fri Feb 07 06:11:44 MST 2014

Quote: LabRat


And how do you debug?



That's a good question. I don't know yet, but I know that some solutions exist.
0 件の賞賛
返信

3,666件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Feb 07 05:37:13 MST 2014

Quote: Gritho
So to be indepedant...



And how do you debug?
0 件の賞賛
返信

3,666件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gritho on Fri Feb 07 05:32:20 MST 2014
Thanks! but...

I used to use LPCXpresso, but I had several problems with. So to be indepedant and have the mastering of all the process, I program the LPC11C24 with my own crosscompilation, I used crosstool-ng to create it. Currently I use the UART to flash but I can't debug and that's not the easiest way to flash. It's for these reasons I would like use the SWD but without the constraint of LPCXpresso.
0 件の賞賛
返信

3,666件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Feb 07 04:03:56 MST 2014

Quote: Gritho
Do you have any idea how to use it with archlinux?



It's a good idea to use LPCXpresso & Link2.

http://www.lpcware.com/lpcxpresso/download

User Guide is talking about supported Linux versions:

• Linux – Ubuntu 11 onwards
• Linux – Fedora 17 onwards

Other distributions may run or not...

http://support.code-red-tech.com/CodeRedWiki/RunningOnLinux
0 件の賞賛
返信

3,666件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gritho on Fri Feb 07 03:50:34 MST 2014
HO... ok!

Thank you for your answer and your links!! I will try LPC-Link2.

Do you have any idea how to use it with archlinux?
0 件の賞賛
返信

3,666件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Feb 07 03:00:06 MST 2014
LPC11C24 is not supporting JTAG  :O

The simplest way to debug/flash your 11C24 is a LPC-Link2.

http://www.embeddedartists.com/products/lpcxpresso/lpclink2.php

http://www.watterott.com/de/LPC-Link-2

It's working without problems with LPC11C24 and a simple SWD connection (and faster than a LPC-Link)....
0 件の賞賛
返信