JTAG/SWD Programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JTAG/SWD Programming

跳至解决方案
3,770 次查看
btellefsen
Contributor I

Hello,

I'm hoping to create a board using the LPC11D14 and am curious how exactly the SWD/JTAG header is to be connected to the processor in order to flash the part correctly using an LPC-LINK 2.

I appreciate any help!

标签 (1)
1 解答
3,342 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Please check the image below. 

In addition please check the following thread:

Design Considerations for Debug 

pastedImage_1.png

For debugging purposes, it is useful to provide access to the ISP entry pin PIO0_1. This pin can be used to recover the part from configurations which would disable the SWD port such as improper PLL configuration, reconfiguration of SWD pins as ADC inputs, entry into Deep power-down mode out of reset, etc. This pin can be used for other functions such as GPIO, but it should not be held low on power-up or reset.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
3,343 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Please check the image below. 

In addition please check the following thread:

Design Considerations for Debug 

pastedImage_1.png

For debugging purposes, it is useful to provide access to the ISP entry pin PIO0_1. This pin can be used to recover the part from configurations which would disable the SWD port such as improper PLL configuration, reconfiguration of SWD pins as ADC inputs, entry into Deep power-down mode out of reset, etc. This pin can be used for other functions such as GPIO, but it should not be held low on power-up or reset.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------