J-Link failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

J-Link failure

957 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhall0819 on Wed Sep 17 10:10:29 MST 2014
Hi,

I have an application with an LPC2136 using IAR EWARM 4.3 and an old J-LINK-ARM-KS (before rev numbers were printed on the case) running on an XP platform. It has been working for years.

The product is now moving to the LPC2148 and with that an upgrade to IAR EWARM 7.2 with a newer J-LINK-ARM-KS (hardware V5.4) running on Windows 8.

I am having trouble loading flash for debug from the IAR IDE. I get message saying the RTCK is not there or memory access timeout.

I suspect my JTAG connection is not compatible with the newer J-Links. I have been through the Segger docs - no help. Is there an app note describing how to connect and configure the LPC2136/48 for use with the J-Link?

Thanks
Labels (1)
0 Kudos
Reply
0 Replies