Issue with flashing LPCXpresso54628 EVK board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with flashing LPCXpresso54628 EVK board.

1,970 Views
a_s
Contributor II

Hello, I am trying to flash the controller via UART port using FLASH MAGIC on LPC54628 evk. Below fig. shows the configuration for flash magic:

Screenshot 2025-02-11 182159.png

During first flashing attempt, I accidently erased the whole chip by checking the erase entire device option in flash magic. After this, the device is not getting either in Flash magic or in MCUxpresso IDE. Looks like erasing the entire chip has erased the bootloader as well. 

I am getting following error in MCUxpresso IDE:

a_s_0-1739278676705.png

Error: 0 available SWD Devices detected.


In what way I can recover the MCU from this stage ? 

 

Thank You


OM13098

Labels (2)
0 Kudos
Reply
10 Replies

1,864 Views
a_s
Contributor II

I recall the following scenario:

I successfully flashed the GPIO example code from MCUXpresso-SDK  using MCUXpresso-IDE  without any issues.

When I attempted to flash the same .bin file using the Flash Magic Tool, I followed the user manual instructions. I placed the device in UART ISP mode and executed the ISP commands via a serial terminal, receiving the expected responses. I then used the following configurations in Flash Magic:

a_s_0-1739513572563.png

After performing these steps, the device is no longer detected by either Flash Magic or MCUXpresso-IDE .
I am getting following error in MCUXpresso-IDE  :

a_s_1-1739513572465.png

Error: 0 available SWD Devices detected.

 

In what way I can recover the MCU from this stage ? 

Best regards,
Akshay Sidral

0 Kudos
Reply

1,753 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @a_s

 Have you programmed a GPIO demo without making any changes?

Please put the device back into ISP mode. Then, attempt to perform a full erase using Flash Magic. After that, try debugging again with MCUXpresso IDE. Note that you should switch to a new workspace in MCUXpresso IDE and import a new GPIO demo.

If it still doesn't work, please update the debugger firmware. 

 

BR

Alice

0 Kudos
Reply

1,711 Views
a_s
Contributor II

Hello @Alice_Yang ,
We initially programmed the demo GPIO, and the execution was successful. We also configured the device in ISP mode and attempted to erase the Flash using Flash Magic. However, we encountered the following error:

image.png

Despite trying all the supported baud rates in Flash Magic, the error persists.

Could you kindly guide us on how to proceed with updating the debugger firmware?

Thank you for your assistance, and I look forward to your prompt response.

 

Best regards,
Akshay

0 Kudos
Reply

1,683 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @a_s 

Please refer to the board user manual -> 4.2 Programming the link2 firmware

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true 

update.jpg

 

BR

Alice

0 Kudos
Reply

1,648 Views
a_s
Contributor II

Hello @Alice_Yang,

I have gone through the link which you have attached, but page is not available:image.png

Then I have referred User Manual, the mentioned link is also not available :
http://www.nxp.com/lpcutilities


image.png

Is there any other source for the document? 

Kindly help on this ASAP as we are unable to use the evaluation board. 

 

Best Regards,

Akshay

0 Kudos
Reply

1,624 Views
Alice_Yang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,925 Views
samv
Contributor II

Do you have an LPC-Link2 board available?  That may get you into the chip via the JTAG/SWD port.

If not, might be a worthwhile investment.

Good luck. 

 

0 Kudos
Reply

1,898 Views
a_s
Contributor II

Thank your for the reply.

At the moment, we are getting it in couple of days. Could you pin point the root cause of this problem ? How did the boot ROM got erased ? 

Thank you for your assistance.

 

Best regards,
Akshay Sidral

0 Kudos
Reply

1,886 Views
samv
Contributor II

Remember to follow the procedure for using the external probe in the user manual.

0 Kudos
Reply

1,887 Views
samv
Contributor II

I don't suspect the ROM was erased (ROM = Read Only Memory) but rather the on-board debug probe got corrupted.  I am not an expert in this area but it's my best guess.

Hopefully you will make some progress.

 

 

0 Kudos
Reply