Issue with USBisConfigured()

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with USBisConfigured()

1,102件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by esheets on Fri Oct 30 15:39:48 MST 2015
So I am currently using custom hardware with a LPC1549JBD48. I am trying to get the LPC Open generic mouse project to run on it. The device is bus powered, and I just want to make sure it is possible to run this program. From what I see, the only thing that really needs to be changed is the VBUS connection. Now I'm always getting False when I get to the USBisConfigured portion of the code. Do I just need to set the VBUS high for the device to know it is powered, or is there something else I am missing. I can get the device to show on my laptop as 15xx Mouse, but not able to send reports since it never gets past the isConfigured portion and just sets itself to busy.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)