Issue with LP2364 UART communication

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with LP2364 UART communication

951 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NeethuG on Wed Oct 14 01:36:33 MST 2015
Dear All,

I am trying to implement UART0 communication in LPC2364.

I am using Sample Code Bundle for LPC23xx/LPC24xx Peripherals using Keil's μVision downloaded from the link 
https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-%C...

In start up code OSCEN is set but when we check the "System control and status" window, the register is found reset.

I am not able to set a desired baud rate also.

There is problem with interrupt also... Interrupt is getting fired but its not entering into start up code.


Please give your valuable suggestions

标签 (1)
0 项奖励
回复
0 回复数