Is there any way to detect the reset source of the LPC1785 mcu?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any way to detect the reset source of the LPC1785 mcu?

1,502 次查看
hongjianzhang
Contributor III

Recently many our boards didn't work well, the phenomenon is some board began to reset all the way when the MCU is  first in deep sleep mode and second wake up from IO then third we use the watchdog illegal command to reset the MCU to reset all our application.  we want to make sure which of the reset source lead to the mcu reset.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,182 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread

Internal RAM to determine cause of core reset 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复