Is possible to program a lpc1769 via raspberry?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is possible to program a lpc1769 via raspberry?

1,700 次查看
davidzamudio
Contributor I

The LPCXpresso IDE for Linux available to download on NXP page is no compatible with raspbian, but Eclipse IDE can run on raspbian.

标签 (1)
0 项奖励
回复
2 回复数

1,450 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi David Zamudio,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

Maybe you can try the MCUXpresso IDE whose link is below.

MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE)|NXP
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,450 次查看
davidzamudio
Contributor I

Hello jeremyzhou‌, thanks for the answer
I'll copy past the terminal output after to run Linux MCUXpresso Installer


dpkg: error al procesar el archivo mcuxpressoide-10.2.0_759.x86_64.deb (--install):
la arquitectura del paquete (amd64) no corresponde con la del sistema (armhf)


Did you know spanish? Its easy :smileyhappy:

Someone tell me about to compile mi object and upload it to the lpc's flash by serial. I'm looking about it right now

0 项奖励
回复