Is posible use SWDIO pin PIO1_3 like GPIO and reprogrammer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is posible use SWDIO pin PIO1_3 like GPIO and reprogrammer?

1,320 Views
alainarri
Contributor I

Is posible use SWDIO pin PIO1_3 like GPIO and reprogrammer?

I reprogramming LPC11C24 controller on my firmware use PIO1_3(SWDIO) like GPIO. Posteriorly microcontroller can't reprogramming.

Labels (1)
0 Kudos
Reply
2 Replies

1,117 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Alain Arri ,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

1) Is posible use SWDIO pin PIO1_3 like GPIO and reprogrammer?

    I think so, you can share some codes about the demo and it can help me to work it out.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,117 Views
alainarri
Contributor I

gpio initialization code:

#include "gpio.h"

#define outRS485EN_port 0   //
#define outRS485EN_pin 0    //

#define outPIN0_port 1   //
#define outPIN0_pin 1    //

#define outPIN1_port 1   //
#define outPIN1_pin 2    //

#define outPIN2_port 1   //
#define outPIN2_pin 3    //

#define outPIN3_port 1   //
#define outPIN3_pin 4    //

#define outPIN4_port 3   //
#define outPIN4_pin 0    //

#define outPIN5_port 3   //
#define outPIN5_pin 1    //

#define outPIN6_port 3   //
#define outPIN6_pin 2    //

#define outPIN7_port 3   //
#define outPIN7_pin 3    //

#define inPIN0_port 1   //
#define inPIN0_pin 0    //

#define inPIN1_port 1   //
#define inPIN1_pin 5    //

#define inPIN2_port 1   //
#define inPIN2_pin 8    //

#define inPIN3_port 2   //
#define inPIN3_pin 0    //

#define inPIN4_port 2   //
#define inPIN4_pin 1    //

#define inPIN5_port 2   //
#define inPIN5_pin 2    //

#define inPIN6_port 2   //
#define inPIN6_pin 3    //

#define inPIN7_port 2   //
#define inPIN7_pin 6    //

void gpio_init(void)
{
    //Configuramos los pines del puerto serie UART
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_6, (IOCON_FUNC1 | IOCON_MODE_INACT));/* RXD */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_7, (IOCON_FUNC1 | IOCON_MODE_INACT));/* TXD */

    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_0, (IOCON_FUNC1 | IOCON_MODE_INACT));/*Dig input PIN0 input */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_5, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig input PIN1 input */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_8, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig input PIN2 input */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_0, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig input PIN3 input */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_1, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig input PIN4 input */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_2, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig input PIN5 input */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_3, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig input PIN6 input */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_6, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig input PIN7 input */

    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_1, (IOCON_FUNC1 | IOCON_MODE_INACT));/*Dig output PIN0 outptu */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_2, (IOCON_FUNC1 | IOCON_MODE_INACT));/*Dig output PIN1 outptu */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_3, (IOCON_FUNC1 | IOCON_MODE_INACT));/*Dig output PIN2 outptu */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO1_4, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig output PIN3 outptu */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO3_0, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig output PIN4 outptu */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO3_1, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig output PIN5 outptu */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO3_2, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig output PIN6 outptu */
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO3_3, (IOCON_FUNC0 | IOCON_MODE_INACT));/*Dig output PIN7 outptu */

    //configurar I2C
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO0_4, IOCON_FUNC1 | I2C_FASTPLUS_BIT);
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO0_5, IOCON_FUNC1 | I2C_FASTPLUS_BIT);

    //configuramos el pin de enable del rs485
    Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO0_0, (IOCON_FUNC1 | IOCON_MODE_INACT));/*Como salida*/
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outRS485EN_port, outRS485EN_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outRS485EN_port, outRS485EN_pin, false);
    //configuramos pines de salida puerto digital, todas las salidas a 0vdc
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN0_port, outPIN0_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN0_port, outPIN0_pin, false);
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN1_port, outPIN1_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN1_port, outPIN1_pin, false);
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN2_port, outPIN2_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN2_port, outPIN2_pin, false);
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN3_port, outPIN3_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN3_port, outPIN3_pin, false);
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN4_port, outPIN4_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN4_port, outPIN4_pin, false);
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN5_port, outPIN5_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN5_port, outPIN5_pin, false);
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN6_port, outPIN6_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN6_port, outPIN6_pin, false);
    Chip_GPIO_SetPinDIROutput(LPC_GPIO, outPIN7_port, outPIN7_pin );
    Chip_GPIO_WritePortBit(LPC_GPIO, outPIN7_port, outPIN7_pin, false);

    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN0_port, inPIN0_pin );
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN1_port, inPIN1_pin );
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN2_port, inPIN2_pin );
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN3_port, inPIN3_pin );
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN4_port, inPIN4_pin );
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN5_port, inPIN5_pin );
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN6_port, inPIN6_pin );
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, inPIN7_port, inPIN7_pin );

main:

void UART_IRQHandler(void)
{
    IRQPC(&PCDataValue);
}

int main(void)
{
    //uint8_t a;
    SystemCoreClockUpdate();
    // Set up and initialize all required blocks and
    // functions related to the board hardware
    Board_Init();

    //WatchdogInitialize();
    Chip_WWDT_Feed(LPC_WWDT);
    gpio_init();//< GPIO initialization.

    //inicializar uart
    initPC(&PCDataValue);

    //iniciar puerto I2C
    init_I2C();
    // TODO: insert code here
    initCPU();

    // Enter an infinite loop, just incrementing a counter
    while(1)
    {
        Chip_WWDT_Feed(LPC_WWDT);
        //printf("while\n");
        if(PCDataValue.flgDataToRead==true)
        {
            //printf("Datos recibidos\n");
            if(readPCdata(&PCDataValue)==true)
            {
                //miramos si el ID de unidade de test corresponde con el recibido por el puerto serie
                if(IdUnitTest==PCDataValue.lIdUnitTest)
                {
                    //miramos el mensaje para que PCB corresponde
                    switch(PCDataValue.IdPCB)
                    {
                        case 0x01://corresponde a la placa CPU
                            comandoCPU(&PCDataSend, &PCDataValue);
                            break;
                        case 0x02:
                            comandoAlaogIO(&PCDataSend, &PCDataValue);
                            break;
                    }
                    sendDataPC(&PCDataSend);
                }
            }
            else
            {
                if(IdUnitTest==PCDataValue.lIdUnitTest)
                {
                    //devolver error
                    PCDataSend.lIdUnitTest=IdUnitTest;
                    PCDataSend.IdPCB=0x01;
                    PCDataSend.Command=0x0001;
                    PCDataSend.dataLength=1;
                    if(PCDataValue.flgCRCError==true)
                        PCDataSend.Data[0]=ERROR_CRC;
                    else
                        PCDataSend.Data[0]=ERROR_GENERAL;
                    sendDataPC(&PCDataSend);
                }
            }
        }
    }
    return 0 ;
}

0 Kudos
Reply