Is it possible to use webserver application without using RTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use webserver application without using RTOS

2,525件の閲覧回数
prasanthapplied
Contributor III

Dear all,

        I'm using lpc1768 microcontroller and i want to act as a webserver and tcp client. I need to know this is possible without using RTOS or not. Please respond me as soon as possible.

Thanks & Regards,

Prasanth.

ラベル(1)
タグ(2)
2 返答(返信)

2,361件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

You can implement this without RTOS, but it is not an easy work. I suggest to use an stack for this, for example LWIP that is included in LPCOpen.

LPCOpen is extensive collection of free software libraries (drivers and middleware) and example programs that enable developers to create multifunctional products based on LPC microcontrollers.

You can download it from the next link(LPCXpresso LPC1769 board):

LPCOpen Libraries and Examples|NXP

After download it you will find some examples that you can use as reference.

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,361件の閲覧回数
prasanthapplied
Contributor III

Dear Soledad,

        Thanks for your reply. From that example codes i can found webserver example which is what i want.

       But the only problem is that example simply have just one line of web page. I expect some more than one page and put,get data from a webpage. Please assist me to do this.

Thanks & Regards,

Prasanth.

0 件の賞賛
返信