Is it possible to use internal flash memory to store data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to use internal flash memory to store data?

1,399 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ANAS MUBARAK on Sun Apr 27 05:08:30 MST 2014

"Is it possible to use LPC1114 internal flash memory to store variable data?"

Is anyone can help me?


thanks

ANAS MUBARAK
Labels (1)
0 Kudos
Reply
2 Replies

1,366 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ANAS MUBARAK on Sun Apr 27 05:35:45 MST 2014

THANKS
0 Kudos
Reply

1,366 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Apr 27 05:15:52 MST 2014

Quote: ANAS MUBARAK
"Is it possible to use LPC1114 internal flash memory to store variable data?"



Yes, use IAP.

There are several examples posted already....

http://www.lpcware.com/content/blog/application-programming-iap-code-example


0 Kudos
Reply