Is it possible to use internal flash memory to store data?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use internal flash memory to store data?

1,396件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ANAS MUBARAK on Sun Apr 27 05:08:30 MST 2014

"Is it possible to use LPC1114 internal flash memory to store variable data?"

Is anyone can help me?


thanks

ANAS MUBARAK
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,363件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ANAS MUBARAK on Sun Apr 27 05:35:45 MST 2014

THANKS
0 件の賞賛
返信

1,363件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Apr 27 05:15:52 MST 2014

Quote: ANAS MUBARAK
"Is it possible to use LPC1114 internal flash memory to store variable data?"



Yes, use IAP.

There are several examples posted already....

http://www.lpcware.com/content/blog/application-programming-iap-code-example


0 件の賞賛
返信