Is it possible to communicate with more than one Device using TCP/IP communication through LPC1768 Based controller Board???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to communicate with more than one Device using TCP/IP communication through LPC1768 Based controller Board???

1,395件の閲覧回数
chithraks
Contributor I

I would like to get excuse from all of you before Explaining my issue. It may look so simple for you all. But as I am new to the world of Ethernet communication using controllers no other option for me to get solution rather than this.

We are using an LPC1768 Based controller Board with a Ethernet Port. LPCXpresso is the IDE we are working with. I am working with TCP/IP protocol right now. I am looking for a solution to my problem.

  1. The controller is used to communicate with A camera and one more Device, All the 3 in the Same network.
  2. Both Based on TCP/IP protocol.
  3. I have to send few commands for controlling the functionality of both through TCP/IP as  I mentioned earlier. Few commands will Reply with some data's (A two way communication is requires were Controller Board acting as Master and both Devices as Slave)
  4. Using Easyweb Library I could communicate with one at a time
  5. I cant give Dedicated Boards to control  them separately.
  6. I need some one to Help me to come out from the issue.
  7. Suggest a Library for my Requirement which can send data to 2 different IP address Devices.
  8. I should be able to address two devices and I have to get connected with both devices for Sending and Receiving Packets
  9. If the controller we use have any limitations Suggest me a better option to achieve my Goal
  10. Thank you all in advance. !
0 件の賞賛
返信
1 返信

1,266件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

It is possible, however we don´t have an example like you need however you can check the below threads as reference:

Can't get more than 3 active TCP connections - Question | mbed 

EthernetInterface Library | mbed 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信