Is eMMC supported on LPC54608?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is eMMC supported on LPC54608?

1,609件の閲覧回数
padraig_fogarty
Contributor III

Just wondering of anyone can tell if eMMC is supported on the LPC54608 device?

The user manual suggests that it is,"One SD or MMC (4.4), CE-ATA (1.1), or eMMC (4.4) device."

however the datasheet doesn't refer to eMMC and suggests a different MMC version (4.1)

Any clarification would be much appreciated.

ラベル(1)
1 返信

1,483件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

On LPC546XX, SDMMC interface supports One SD or MMC (4.4), CE-ATA (1.1), or eMMC (4.4) device.

There is a difference on MMC version instead of eMMC between UM and DS. I will report the issue to our documentation team.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------