Is display extension kit compatible with lpc4357 developers kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is display extension kit compatible with lpc4357 developers kit

1,145 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pramodh on Mon Sep 07 05:50:34 MST 2015
Hello,

I have been working with LPC4088 Experiment baseboard and the Display Expansion Kit (5 inch) till now. I have recently bought a LPC4357 Developers kit. Is it possible to use the same Display extension kit with the new LPC4357 board,since the display kit has a parallel RGB interface (FFC - Flexible Flat Cable) and for lpc4357, a 2x25 IDC connector (2.54mm pitch) is used to interface the display board. Is there any adapter or converter available? or should i buy a LCD Board, 4.3 inch TFT 480x272) ? Thanks in advance.

Reference links :
http://www.embeddedartists.com/products/displays/disp_exp_50.php
http://www.embeddedartists.com/products/displays/lcdb_43.php

Regards
Pramodh
Labels (1)
0 Kudos
Reply
0 Replies