Is VBUS input required for device mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is VBUS input required for device mode?

8,074 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdupre on Mon Jul 15 10:20:28 MST 2013
I have a LPC17xx system with USB2 configured as host.  I'd like USB1 to be in device mode.  Unfortunately, USB_PWRD2 and USB_VBUS are on the same pin.

User Manual indicates that USB_VBUS is internally pulled high when pin is not assigned to that function.  Does this just mean that the USB device system will always think that the device is connected?

In my case, the USB device port will either be connected to a power supply, or to a computer.  (i.e the system gets power from the USB device port in all cases-- there is no other power supply.)  Do I really need to detect VBUS for USB device mode to work?
标签 (1)
0 项奖励
回复
1 回复

7,275 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tsuneo on Tue Jul 16 03:09:52 MST 2013

Quote:
User Manual indicates that USB_VBUS is internally pulled high when pin is not assigned to that function. Does this just mean that the USB device system will always think that the device is connected?


Yes.
It's fine for bus-powered devices, because the running firmware means that the bus power is supplied. There is no need to detect VBUS voltage explicitly at the USB connector.

For self-powered devices, however, VBUS detection is necessary. Just while VBUS voltage presents, D+ pull-up resistor (ie. USB_CONNECT) is enabled, as the requirement of USB2.0 spec (*1). Also VBUS detection is required to suppress spurious USB interrupts by floating D+/D- lines.


(*1) 7.1.5.1 Low-/Full-speed Device Speed Identification (on usb_20.pdf)
The voltage source on the pull-up resistor must be derived from or controlled by the power supplied on the USB cable such that when VBUS is removed, the pull-up resistor does not supply current on the data line to which it is attached.


Tsuneo
0 项奖励
回复