Is Texas Instruments Ethernet PHY Layer Transceiver DP83822 compatible with LPC4088FBD144 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is Texas Instruments Ethernet PHY Layer Transceiver DP83822 compatible with LPC4088FBD144 ?

2,285 Views
sunilsawant
Contributor I

I want to connect Texas Instruments DP83822 PHY Layer Ethernet transceiver with LPC4088FBD144.

Can the said Ethernet transceiver work with LPC4088FBD144 ?

Labels (1)
0 Kudos
Reply
3 Replies

1,954 Views
sunilsawant
Contributor I

Thank you for promptly answering my question.

To be specific, I am using DP83822HF Ethernet PHY transceiver. Will the said transceiver be compatible with LPC4088FBD144 ?

I am asking this question because, DP83822HF has more features than basic DP83822. So would all the features in DP83822HF be supported by LPC4088FBD144 ?

0 Kudos
Reply

1,954 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Sunil Sawant,

Thanks for your reply.

My answer is yes, as the Ethernet block contains a full featured 10 Mbps or 100 Mbps Ethernet MAC (Media
Access Controller) designed to provide optimized performance through the use of DMA hardware acceleration.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,954 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Sunil Sawant,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Yes, LPC4088FBD144 can definitely work with the DP83822.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply