Interrupt Priority

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt Priority

Jump to solution
3,168 Views
Dhaya
Contributor III

Hi, 

    Here we using multiple interrupts including externa, I2C, Timers,.. During run time, some of the interrupts has been disabled and enable as per the application needs. So my doubt is, when the priority of the interrupt has to assigned. During enable of interrupt or during initialization or set all peripheral interrupts in one by one manners

0 Kudos
Reply
1 Solution
3,159 Views
ErichStyger
Specialist I

In principle, you can do it anytime.

Just keep in mind that the architecture might have some delays/caches, so you need to add memory barriers, as explained in https://mcuoneclipse.com/2015/10/16/nvic-disabling-interrupts-on-arm-cortex-m-and-the-need-for-a-mem...

As for myself, I initialize interrupts during the device/peripheral setup, one by one, with the global interrupts disabled. At the end, with starting the application or the RTOS, the global interrupts get enabled.

If disabling/enabling interrupts during the runtime is needed for example for re-entrancy reasons, then you could possibly manage this with proper interrupt grouping and priority mapping. The challenge with disabling certain interrupts at runtime might make it more complex to verify and validate that the system is operating as desired, but that depends of course on the stuff you are doing.

I hope this helps,

Erich

 

PS: You might have a read at a series about ARM Cortex interrupts:

https://mcuoneclipse.com/2016/08/14/arm-cortex-m-interrupts-and-freertos-part-1/

https://mcuoneclipse.com/2016/08/20/arm-cortex-m-interrupts-and-freertos-part-2/

https://mcuoneclipse.com/2016/08/28/arm-cortex-m-interrupts-and-freertos-part-3/

 

View solution in original post

1 Reply
3,159 Views
ErichStyger
Specialist I

In principle, you can do it anytime.

Just keep in mind that the architecture might have some delays/caches, so you need to add memory barriers, as explained in https://mcuoneclipse.com/2015/10/16/nvic-disabling-interrupts-on-arm-cortex-m-and-the-need-for-a-mem...

As for myself, I initialize interrupts during the device/peripheral setup, one by one, with the global interrupts disabled. At the end, with starting the application or the RTOS, the global interrupts get enabled.

If disabling/enabling interrupts during the runtime is needed for example for re-entrancy reasons, then you could possibly manage this with proper interrupt grouping and priority mapping. The challenge with disabling certain interrupts at runtime might make it more complex to verify and validate that the system is operating as desired, but that depends of course on the stuff you are doing.

I hope this helps,

Erich

 

PS: You might have a read at a series about ARM Cortex interrupts:

https://mcuoneclipse.com/2016/08/14/arm-cortex-m-interrupts-and-freertos-part-1/

https://mcuoneclipse.com/2016/08/20/arm-cortex-m-interrupts-and-freertos-part-2/

https://mcuoneclipse.com/2016/08/28/arm-cortex-m-interrupts-and-freertos-part-3/