Internal Vref for ADC in LPC802

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Internal Vref for ADC in LPC802

Jump to solution
2,027 Views
asier
Contributor III

Hi,

I want to use ADC with 1V positive reference. My VCC is 3V3. 

I can see VREFP input for external positive reference but is there any internal Vref like in ACOMP module ?

Thanks, 

Asier.

Labels (1)
0 Kudos
Reply
1 Solution
1,969 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Asier,

Only the ACOMP module has an internal reference, so the ADC does require that you use the external reference.

My apologies for the inconvenience.

Regards,
Gustavo

View solution in original post

0 Kudos
Reply
1 Reply
1,970 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Asier,

Only the ACOMP module has an internal reference, so the ADC does require that you use the external reference.

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos
Reply