Interfacing touch screen lcd with LPC1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing touch screen lcd with LPC1769

1,716件の閲覧回数
ashinde555
Contributor I

I was trying to interface a touch screen display with lpcxpresso lpc1769

I am using waveshare 5" with xpt2046 touch controller, but it has HDMI port for display.

How can interface this display with lpc1769.

Pls help.

ラベル(1)
0 件の賞賛
返信
1 返信

1,709件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Aniket,

 

xiangjun_rong_0-1606113137477.pngxiangjun_rong_0-1606113137477.png

 

From above timing, you can use spi interface of LPC1769 as master to access the xpt2046. You can use the byte length to write and read.  If you use Busy signal, you can connect the Busy to a GPIO, you can read the logic of Busy, after it becomes low, you can write the spi transmit register to launch transfer so that you can read the ADC sample.

Hope it can help you

BR

XiangJun Rong

 

 

0 件の賞賛
返信