Interfacing LPC4357 controller with DDC Total ACE 1553 Chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing LPC4357 controller with DDC Total ACE 1553 Chip

1,400件の閲覧回数
shreelaxminair
Contributor I

hello

We are interfacinge LPC4357 controller with DDC total ACE 1553 chip, BU 648x using EMC. However connection of certain signals are unclear. Can anyone advise over this? 

タグ(1)
0 件の賞賛
返信
1 返信

1,323件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately I don't have experience with the DDC total ACE 1553 chip, however you can use the following application note as reference, this application note describes how to properly interface SDRAM memory to the LPC1800 and LPC4300 External Memory Controller.

https://www.nxp.com/docs/en/application-note/AN11508.pdf 

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信