Instruction Trace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Instruction Trace

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri May 02 09:17:17 MST 2014
UM is promising Instruction Trace:


Quote:
43.2 Features
...
• Trace port provides CPU instruction trace capability. Output via a Serial Wire Viewer.
...


LPCXpresso Help doesn't list LPC15xx as supported target:

Quote:

Supported targets
Instruction Trace is not supported on all targets. It only works on targets which have the necessary hardware.
Instruction trace is currently supported on the following targets from NXP:

LPC8xx (MTB)

LPC11U6x (MTB)

LPC18xx (ETM / ETB)

LPC43xx (ETM / ETB)



So does LPC15xx not provide Instruction Trace or isn't it implemented in LPCXpresso?
ラベル(1)
0 件の賞賛
返信
1 返信

1,227件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri May 16 11:47:27 MST 2014
Hi,


The trace pins does not come out of the package and hence it does not support Instruction trace.
The UM will be updated and a new revision will be posted soon.

Thanks,
NXP Technical Support
0 件の賞賛
返信