Infrared configuring in lpc3250

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Infrared configuring in lpc3250

1,361 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akarshana on Wed Jan 01 21:52:51 MST 2014
hai

In my project I want use LPC3250-IR_RX pin,

Is there any configuration required in kernel? If it is can any one tell me how to configuring kernel,

and what is the data format while reading this pin?

Is there any example code for IRDA communication

thank you advance

Labels (1)
0 Kudos
Reply
2 Replies

1,305 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embeddedguy on Tue Mar 18 10:14:06 MST 2014
t
0 Kudos
Reply

1,305 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Feb 06 16:32:46 MST 2014
Hi Akarshana,

Visit the following link for examples on IrDA in the UART  folder for LPC175x/6x.

http://www.lpcware.com/content/nxpfile/lpc175x6x-cmsis-compliant-standard-peripheral-firmware-driver...


Thanks

NXP Technical Support
0 Kudos
Reply