Information about CTIMER module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Information about CTIMER module

2,528件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Is the ctimer counter always on? Even when debugger is in halt state?

0 件の賞賛
返信
2 返答(返信)

2,428件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Mahesh

If you are using MCUXpresso and the SWD tool, basically there is no HALT button, there is  PAUSE and STOP if the debug it is in STOP the register are in last state that the Software provide, this means the MCU it is not running neither the peripherals all clocks are out.

Regards,

Sol  

0 件の賞賛
返信

2,337件の閲覧回数
phatpaul
Contributor III

Hi, I have the same question as OP.  But your response isn't clear.

I'm trying to debug my code which uses the CTIMER to interrupt on compare match.  But it seems like the timer is still counting in the background if I pause or hit a break-point.

On Kinetis, the timer pauses when the program is paused.  Can we do that on LPC804's CTimer also?

0 件の賞賛
返信