Increase drive strength for UART in NXP LPC54S018

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Increase drive strength for UART in NXP LPC54S018

1,224件の閲覧回数
robo_v
Contributor I

 

How to increase the drive strength for UART in NXP LPC54S018 Microcontroller.

We are observing CRC erorrs due to which we want to increase drive strength and check once

 

0 件の賞賛
返信
1 返信

1,213件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The LPC54xxx does not have high driving or low driving mode, all of the pins has standard mode.

But there is slew bit for each pin, you can set the slew bit, which means the fast rising/falling edge, accordingly, the driving strength becomes high.

xiangjun_rong_0-1705913645432.png

 

As you know that the CRC does not have external pin, it appears that the CRC error does not relate to the pin attribute.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信