ISR Handling Problem with lpc 2368

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISR Handling Problem with lpc 2368

790件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jijo on Thu Oct 08 03:44:50 MST 2015
Hi,
I have problem with ISR Handling in LPC 2368.
In my program , the program  did not switch to isr function  when interrupt fired. But in the vector interrupt control table it shows the the interrupt request.

what are the reason for this type of issue ?
Is there any problem with startup code ?
Is there any way for to investigate the reason?
ラベル(1)
0 件の賞賛
返信
0 返答(返信)