ISP programming lpc4430

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISP programming lpc4430

3,342 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kumarbhimesh on Wed Dec 17 01:47:03 MST 2014
Hi,

I am newbie to lpc. We have custom made lpc4430 board with external flash.

We need to flash the external flash using ISP programmer.

Can you suggest me Hardware and Software tools and any documentation for flash procedure.


Regards,
Bhimesh.
Labels (1)
0 Kudos
Reply
2 Replies

3,248 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kumarbhimesh on Wed Dec 17 02:30:28 MST 2014


Hi,

Thank you so much for the support.

please let me know hardware tool to flash.

Micro controller  : LPC4330FET180

External Flash : N25Q064A13ESE40E

Boot mode is USART0 with P2_7 pin is low.


Regards,
Bhimesh.
0 Kudos
Reply

3,248 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Wed Dec 17 02:16:46 MST 2014
Use Flash Magic for serial programming:

http://www.flashmagictool.com/

Select the external flash (I assume you used a qSPI flash) as shown in the attached picture.


You can also use the USB port for ISP, please look here:

http://www.lpcware.com/content/nxpfile/nxp-lpc18xx43xx-dfu-download-and-secure-image-generator

Regards,
NXP Support Team
0 Kudos
Reply