ISP programming lpc4430

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ISP programming lpc4430

3,335 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kumarbhimesh on Wed Dec 17 01:47:03 MST 2014
Hi,

I am newbie to lpc. We have custom made lpc4430 board with external flash.

We need to flash the external flash using ISP programmer.

Can you suggest me Hardware and Software tools and any documentation for flash procedure.


Regards,
Bhimesh.
标签 (1)
0 项奖励
回复
2 回复数

3,241 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kumarbhimesh on Wed Dec 17 02:30:28 MST 2014


Hi,

Thank you so much for the support.

please let me know hardware tool to flash.

Micro controller  : LPC4330FET180

External Flash : N25Q064A13ESE40E

Boot mode is USART0 with P2_7 pin is low.


Regards,
Bhimesh.
0 项奖励
回复

3,241 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Wed Dec 17 02:16:46 MST 2014
Use Flash Magic for serial programming:

http://www.flashmagictool.com/

Select the external flash (I assume you used a qSPI flash) as shown in the attached picture.


You can also use the USB port for ISP, please look here:

http://www.lpcware.com/content/nxpfile/nxp-lpc18xx43xx-dfu-download-and-secure-image-generator

Regards,
NXP Support Team
0 项奖励
回复