ISP pins with external SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISP pins with external SDRAM

1,159件の閲覧回数
lpelton
Contributor I

The ISP boot pins are multiplexed with external bus interface data pins.  I'm having a problem where resetting the chip sporadically results in the LPC54608 getting stuck in the NXP bootloader.  As far as I can tell, the SDRAM pins which are multiplexed with ISP0-ISP2 are high impedance when this happens, because DQML is high.

Is this a known problem/error with the boot process?  Disabling entry to ISP using the ISP pins via an OTP memory setting is an option that I've seen listed in another thread, but that doesn't seem like a good solution to me.  Is it possible to reliably use the ISP pins for ISP entry in an LPC54608 design which uses an external memory?

0 件の賞賛
返信
1 返信

1,108件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Larry Pelton ,

I think you'd better disable ISP, or it is easy to enter ISP mode when the pins are multiplexed.

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信