ISP option requirement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISP option requirement

3,136件の閲覧回数
prachipanse
Contributor III

Hi,

Is there a suitable document or link available where the requirement and usage of ISP programming mode is explained?

Also, for the case when this mode is not required to be used for LPC1313, how can that be achieved?

Thanks and Regards,

Prachi 

0 件の賞賛
返信
4 返答(返信)

2,918件の閲覧回数
ckphua
NXP Employee
NXP Employee

Please read the User Manual -chapter 21

http://www.nxp.com/documents/user_manual/UM10375.pdf

There you will find the details of ISP programming mode explanation. 

If your application do not require the ISP,  make sure PIO0_1 pin is not tied to low during power on.

0 件の賞賛
返信

2,918件の閲覧回数
prachipanse
Contributor III

Thanks. So, for programming the flash in LPC1313 is possible only through the UART interface and is not possible if we are using only the SWD port. Can you please confirm my understanding?

Regards,

Prachi 

0 件の賞賛
返信

2,918件の閲覧回数
converse
Senior Contributor V

You can use the lpcxpresso command line flash programming tools to program your device over SWD (as well as directly in the GUI, of course)

https://community.nxp.com/thread/389139 

IIRC, FlashMagic can also be used over SWD as well as UART - but you should double check.

0 件の賞賛
返信

2,918件の閲覧回数
ckphua
NXP Employee
NXP Employee

Yes, only UART ISP for LPC1313.

0 件の賞賛
返信