ISP MODE on LPC5516

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,423件の閲覧回数
claudiobrunelli
Contributor II

When the LPC55 enters ISP mode, it is possible to use the internal bootloader to update the firmware. The communication port is USB.

Is it possible to address the boot to a different serial port and not just the USB?

Thanks in advance.

Claudio

ラベル(1)
0 件の賞賛
返信
1 解決策
4,404件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @claudiobrunelli 

Besides USB ISP mode, LPC55 also support  SPI/I2C/UART ISP mode. Please see this article written by my colleague. Hope this will help you.

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55-Update-Firmware-in-USB-UART-SPI-I2... 

Have a nice day,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,405件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @claudiobrunelli 

Besides USB ISP mode, LPC55 also support  SPI/I2C/UART ISP mode. Please see this article written by my colleague. Hope this will help you.

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55-Update-Firmware-in-USB-UART-SPI-I2... 

Have a nice day,

Jun Zhang

0 件の賞賛
返信
4,387件の閲覧回数
claudiobrunelli
Contributor II
Everything it's ok. Thanks for your suggestion !
0 件の賞賛
返信
4,402件の閲覧回数
claudiobrunelli
Contributor II

Many thanks Jun Zhang for your suggestion.

I'm going to read it. 

 

Claudio

0 件の賞賛
返信
4,054件の閲覧回数
CKONG
Contributor I
Hi Claudio,

I am also looking for procedure and commands to update firmware via ISP mode and SPI interface.

I am using LPC51U68, there are some SH_CMD_xxx commands I can use to update firmware via SPI interface, but I am not sure the detail steps, commands and flash address to use.

If you succeed in ISP mode using non-USB interface, can you share the procedure and commands used with me?

Thank you.

Best Regards,
CK
0 件の賞賛
返信