IR remote controlling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IR remote controlling

2,227 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sharif on Thu Jul 17 22:59:09 MST 2014
Hi all,

i have lpc1227 ,i want control my ac(air conditioner) with my controller board lpc 1227 .

so please suggest me the protocal that is to be used and how can i supposed to start
标签 (1)
0 项奖励
回复
3 回复数

2,124 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Tue Dec 02 15:52:22 MST 2014
See this page for a very good description of the
protocol.
0 项奖励
回复

2,124 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sharif on Sat Nov 22 00:53:21 MST 2014
Thank you ,
my AC has RC5 protocal, can i get any sample codes regarding IR remote for lpc1227
0 项奖励
回复

2,124 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Anthony Xie on Sun Aug 17 23:46:23 MST 2014
Hi, Sharif:

The first thing is needed to get clear about the IR protocol used by this air conditioner.  The RC5,RC6 protocol is popular for a lot of IR device. But for special consumer device (audio, airconditioner, TV, etc) usaully used special IR protocol. Then you can study the IR protocol, and try use MCU to control it. And suggest to use NXP LPC800 to take this role. Because it's low cost and more popular.  Thanks!
0 项奖励
回复