IR remote controlling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IR remote controlling

2,218 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sharif on Thu Jul 17 22:59:09 MST 2014
Hi all,

i have lpc1227 ,i want control my ac(air conditioner) with my controller board lpc 1227 .

so please suggest me the protocal that is to be used and how can i supposed to start
Labels (1)
0 Kudos
Reply
3 Replies

2,115 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Tue Dec 02 15:52:22 MST 2014
See this page for a very good description of the
protocol.
0 Kudos
Reply

2,115 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sharif on Sat Nov 22 00:53:21 MST 2014
Thank you ,
my AC has RC5 protocal, can i get any sample codes regarding IR remote for lpc1227
0 Kudos
Reply

2,115 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Anthony Xie on Sun Aug 17 23:46:23 MST 2014
Hi, Sharif:

The first thing is needed to get clear about the IR protocol used by this air conditioner.  The RC5,RC6 protocol is popular for a lot of IR device. But for special consumer device (audio, airconditioner, TV, etc) usaully used special IR protocol. Then you can study the IR protocol, and try use MCU to control it. And suggest to use NXP LPC800 to take this role. Because it's low cost and more popular.  Thanks!
0 Kudos
Reply